6/26/2023 5:48 PM | |
Joined: 11/17/2022 Last visit: 2/22/2024 Posts: 3 Rating:
|
I'm using WINCC Unified V17 i have a problem to configure IHM Alarms, in my logic in PLC, i use the same Bit to acknowledgment all alarms in motor, but WINCC don't accept use the same bit in 2 or more onces. i use a DWORD called "Status" to triggers os alarms, and other DWORD called "Command", in command DWORD i used bit 16 to acknowledgment of all alarms in same time. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/27/2023 08:56:01New subject after splitting |
|
6/27/2023 8:56 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
Closed cause question posted twice. The second thread with the subject WinCC Unified don't accept to use the same bit in 2 or more onces. is published within the conference WinCC Unified Systems. Jen_Moderator |
Follow us on