Industry Online Support
Technical Forum
2/4/2009 3:19 AM | |
Joined: 9/27/2006 Last visit: 2/9/2025 Posts: 12334 Rating:
|
Hello Swright; Which dropdown menu are you looking at? In Step 7 HWConfig? There are no As-i slaves there... and you do not configure them as you would, for example, DP-slaves.Once addressed, the data of the 32 (or 64) As-i slaves is simply mapped inside a 16-word area in the As-i master's memory area. What manuals are you looking at on the As-i configuration? For example, study chapter 11 in this document for the allocation of bit data of the As-i slaves in the As-i master's layout: http://support.automation.siemens.com/WW/view/en/26250840 There are also chapters on As-i Safe that explain the working principles and how to configure them. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/4/2009 4:54 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on