6/5/2017 2:19 PM | |
Joined: 3/14/2016 Last visit: 4/13/2022 Posts: 7 Rating:
|
Hi, i am trying to configure and simulate the illuminated pushbutton functions for a KTP700F on WinCC Advanced V13.0 SP2 and i am not having much luck. As far as i could understand so far, i will not be able to simulate the LED functions but i need to at least be able to use the buttons to enable functions from the pushbuttons for testing purposes. I've been trying to follow the system manual which has an example for configuration but it seems to me that it has some errors in the examples that are presented (in attachment), and i cannot get it to work. Also, in the system manual it has a table for the availability of Wincc element objects (also in attachment), and for the illuminated pushbutton it seems it is not available for Wincc Runtime advanced. Any Help? Thanks.
AttachmentWCC_Advanced_V13_SP1_enUS_en-US.pdf (214 Downloads) |
Follow us on