5/29/2020 6:25 PM | |
Joined: 10/31/2019 Last visit: 6/14/2024 Posts: 6 Rating:
|
Hello! Help configure OPC in WinCC RT to connect external clients or show an example please. Aleksej. |
5/30/2020 4:25 AM | |
Joined: 7/5/2013 Last visit: 4/17/2025 Posts: 3147 Rating:
|
Hello Aleksej, please see the following FAQ: Communication via OPC UA with SIMATIC HMI systems (Comfort Panels, Runtime Advanced, Runtime Professional) Regards, Frink |
Pi is exactly three! |
|
6/4/2020 12:20 PM | |
Joined: 7/5/2013 Last visit: 4/17/2025 Posts: 3147 Rating:
|
Hello Aleksej, if the PLC is not in the project, you can use a proxy device: Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x or Combined configuration with WinCC (TIA Portal) and STEP 7 (TIA Portel) in separate projects To do it this way, you need the PLC software, either an upload, but better the original source code. Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to
1 thankful Users |
Follow us on