1/2/2019 4:31 PM | |
Posts: 5 Rating: (0) |
Hi Sir, I am trying to configure S120 drive (CONTROL UNIT CU310-2) , I observed following during configration management on wireshark 1. Ident request is OK 2. Controller send connect request to S120 drive. 3. Device rejects connect request with below errors PROFINET IO (Device), Connect Operation: Connect (0) Status: Error: "IODConnectRes", "PNIO", "User specific", "User abort" ErrorCode: IODConnectRes (0xdb) ErrorDecode: PNIO (0x81) ErrorCode1: User specific (255) ErrorCode2: User abort (255) ArgsLength: 0 (0x00000000) Array: Max: 8086, Offset: 0, Size: 0 Any help. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/3/2019 1:34:08 PMNew subject after splitting |
|