Industry Online Support
Technical Forum
3/7/2019 5:23 PM | |
Posts: 2 Rating: (0) |
I try to perform the same operation. with portal v.15, S7-1500, CM1542-5 as DP master and IM157 as DP / PA LINK. in case of using the PDM separately to parameterize the addresses of the instruments. Would I have to connect to the IM157 via PROFIBUS DP using a PG / PCADAPTER and PDM? or some other device is required to configure and start the network. first of all, Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/8/2019 10:22:21 AMNew subject after splitting |
|
Follow us on