12/17/2020 1:50 PM | |
Joined: 2/24/2011 Last visit: 2/25/2025 Posts: 86 Rating:
|
Received an answer from Siemens support: "Contrary to the technical data of the Mobile Panels 1st generation, these devices are still included in WinCC V15 and V15.1. They can be newly created, further modified and also transferred to the hardware. Only with WinCC V16 the devices were finally removed from the WinCC software. Corresponding information can be found in the delivery release for WinCC V16. (point "changed device support"). |
This contribution was helpful to
1 thankful Users |
Follow us on