6/22/2013 1:07 PM | |
Joined: 9/27/2006 Last visit: 3/14/2025 Posts: 12344 Rating:
|
Hello Quantum and Abbas; Maybe you can appreciate the help given by our friends Pegaia and fritz in the following thread: S7-1200 and Profibus PA |
This contribution was helpful to
2 thankful Users |
12/14/2016 10:38 PM | |
Joined: 9/27/2006 Last visit: 3/14/2025 Posts: 12344 Rating:
|
Hello dilan; Have you already followed Mr. Pegaia's suggestion, in the link proposed in a preceding post? Denilson Pegaia Hi, it is possible (as for all DP masters) but it should be generate a GSD with your PA configuration (not so easy). Take a look at How do you connect the IM 157/IM 153-2 in the DP/PA Link to an external master or a SIMATIC S5?(GSD-Tool) http://support.automation.siemens.com/BR/view/en/26562190 Look also at our friend fritz' comments in the same thread, they should help you out. Everything turns on your capacity to generate a custom gsd file for your DP/PA link that will integrate the individual gsd files of all PA instruments in your PA network. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/15/2016 2:25:16 PM |
|
This contribution was helpful to
1 thankful Users |
1/18/2017 1:12 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by Vlad29 is split to a separate thread with the subject Coupler with three Sitrans, can't read PIW "Nr". Best regards |
Follow us on