5/24/2018 3:26 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
The IO-Link is not integrated in TIA Portal and uses an extra tool for the configuration of the IO-Link module: PCT Port Configuration Tool) Mark the CM 4xIO Link module. in the context menu (right mouse Button) you can select the configuration tool (If you find the right entry, the Siemens Port Configuration Tool will open) You will have to import a description file (IODD) of your sensor to PCT. Then you can select in the catalogue inside PCT and set the parameters of your sensor. You have to download the configuration in PCT to the IO-Link modules. See https://support.industry.siemens.com/cs/ww/en/view/65949252 Chapter 3 for details. Maybe you should have a look on this application example too: https://support.industry.siemens.com/cs/ww/en/view/73565887 |
|
|