5/26/2014 10:14 AM | ||||
Joined: 11/21/2007 Last visit: 5/27/2023 Posts: 2321 Rating:
|
Hello AsAPLC Width of Active Bus Module for Power Supply = 97mm Width of 6 Nos. Active Bus Modules for SMs = 6x80 = 480mm Total Width = 577mm These will not fit on 530mm DIN Rain ( 6es7195-1gf30-0xa0 ) You need 620mm DIN Rail : 6ES7195-1GG30-0XA0 - ET200M, RAIL 620MM May be a Bug in the System Configurator Hope this helps Cheers Navnag |
|||
There is no such thing as the last bug in a program |
||||
This contribution was helpful to
2 thankful Users |
5/26/2014 11:25 AM | |
Joined: 3/21/2006 Last visit: 4/12/2023 Posts: 10221 Rating:
|
Very good " calculated " point Navnag! About bug in Configurator perhaps you could make a new thread and everybody who is using that configurator to share...
|
Last edited by: UMENCHO at: 5/26/2014 2:02 PM |
|
5/26/2014 1:32 PM | |
Joined: 11/21/2007 Last visit: 5/27/2023 Posts: 2321 Rating:
|
Thanks UMENCHO BTW - Have you asked Moderator to Hide the "Thanks" button from your posts Dear AsAPLC As suggested by UMENCHO, you should start another thread with the exact details of your problem ( With exact version of Configurator ) so that the Bug if anycan be removed in the next update. Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
5/26/2014 2:16 PM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating:
|
Which configuration tool are u using? TIA Selection tool? |
5/26/2014 2:32 PM | |
Posts: 9 Rating:
|
TIA selection tool 3.0.0.7 but i also checked with the online TIA selction tool with the same result V6.0.1.0
|
5/26/2014 3:42 PM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating:
|
Then it must be a bug in TIA Selection tool. . |
This contribution was helpful to
1 thankful Users |
5/27/2014 5:00 PM | |
Posts: 165 Rating:
|
There are so many bugs in TIA softwares..... but system seems to be stabilize naw a days....
|
This contribution was helpful to
1 thankful Users |
5/27/2014 8:35 PM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating:
|
We can do nothing except hope that programmers at SIEMENS do their jobs error free instead of releasing Service Packs & Updates after a while |
This contribution was helpful to
1 thankful Users |
5/27/2014 9:03 PM | |
Joined: 11/21/2007 Last visit: 5/27/2023 Posts: 2321 Rating:
|
Hello ... Pl see UMENCHO's Post
I can say from my personal experience that they Do Listen and take corrective action which we see in the form of Hotfixes and Service packs Cheers Navnag |
Last edited by: Navnag at: 5/27/2014 9:03 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
Follow us on