Industry Online Support
Technical Forum
4/3/2011 7:00 PM | |
Joined: 3/21/2006 Last visit: 4/12/2023 Posts: 10221 Rating:
|
What kind of error did you receive there? Best regards, Hristo Mihalev |
4/3/2011 9:06 PM | |
Posts: 3 Rating:
|
Hi, I found this error when go online with CP CP Interface not ready CP is switched off or break on cable from PG to CP or break on the interface or wrong path selected in path selection or the wrong interface is set in S5 KOMI I am using the same cable i.e PC/TTY as for S5 PLC which is working fine with PLC but did'nt work with CP1430 TF.I am using the top port of CP i.e AS511 and the file path ,I selected AS511-Mux-EndP I have uploaded some snap shot of my settings. Regards, Denis AttachmentPic2.zip (57 Downloads) |
Follow us on