12/19/2020 3:13 PM | |
Joined: 1/15/2016 Last visit: 4/1/2024 Posts: 2 Rating: (0) |
Hello , I write first time in Siemens forum , please help me . I have an idea to connect 2 absolute encored to my project for motion control task with analog out . I configure the position axis 1 and 2 every think looks good but when I add second encoder i want to compile and shows : PROFIdrive encoder,One encoder has been assigned to multiple axes: Axis_1, Axis_2,,,4:10:53 PM hardware : Siemens s7 1200 1214 dcdcdc analog out module sm1232 and ecndored : MC-ENCODER-Singleturn-13Bit each one . i use telegram 82 Thank you and Best Regards Ramadan Karaali ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2020 10:10:28New subject after splitting |
|
12/22/2020 12:59 PM | |
Joined: 10/11/2006 Last visit: 5/23/2024 Posts: 5852 Rating: (793) |
Hello, it makes no sense to use 1 encoder for 2Technology objects. Only possibility would be to split via data block. 2.2.5 Data connection PROFIdrive drive/PROFIdrive encoder The data connection of PROFIdrive drives and PROFIdrive encoders occurs either directly via the PROFIdrive telegram or via a data block. Use the connection via data block if you want to influence or evaluate telegram contents in the user program for process-specific reasons. 2.2.6 Data connection drive with analog drive connection https://support.industry.siemens.com/cs/ww/en/view/109773400 |
With best regards, |
|