5/13/2014 5:32 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Hello,
We need to know exactly if you connected to your CPU via Profibus or Profinet networks? _____ You have two things to do to establish communication between two OPs and CPU at the same time:
Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
5/13/2014 10:14 PM | |
Posts: 784 Rating: (52) |
Hello, From the control panel: 1- To change IP address:possible . 2- To change profibus address:not possible. Best regards....... |
5/14/2014 9:10 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
Have a look on followinglink Look into 6.14
|
Last edited by: Madhava at: 5/14/2014 2:06 PMLast edited by: Madhava at: 5/14/2014 9:38 AM |
|
5/14/2014 9:23 AM | |
Posts: 433 Rating: (48) |
Your link is not correct. Could you check it please? |
5/14/2014 9:37 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
Sorry. Please find the right onehere.
|
Last edited by: Madhava at: 5/14/2014 2:07 PM |
|
5/14/2014 10:08 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
Hi Ayman, Is it possible to change the address of another OP which is running ?
|
5/14/2014 2:00 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Dear Madhava As has been Correctly pointed out by Ayman Elotaify, the MP will always reset the Profibus address to what has been programmed in the Loaded Project, everytime the project runs. Therefore even if you change the profibus address in the control panel, it will be overwritten when the MP goes to Project "RUN" mode. Just for example, if we set a profibus address in the HMI for downloading the project, once the project is download and "RUN" the manually set address is overwritted by the address ( and other settings ) in the project. In my openion, you have only two options : a) Either get hold of the original project ( Not an Uploaded image ) from the person / company who programmed the HMI, change the profibus address and download to the MP. b) Try to upload the image from the faulty MP. Sometimes this is possible, even if the display has failed but rest of the unit is working. Hope this helps Cheers Navnag |
Last edited by: Navnag at: 5/14/2014 2:04 PMThere is no such thing as the last bug in a program |
|
Follow us on