10/10/2006 4:49 PM | |
Posts: 20 Rating: (0) |
Hi, Could I connect 2 panels on a CPU with 1 AS511 interface ? Thank you for your answers. Best regards |
10/18/2006 1:44 PM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, Which panels do you have in mind? According to chapter 3 of the manual Communication it is only possible when you use panels in the loop-through operation. In loop-through operation, a second operating unit or a PU/PC is connected to the second interface of the operating unit that is connected to the PLC. In all other situations it is one panel on one AS511-port. |
Smurf |
|
Follow us on