8/8/2012 9:40 PM | |
Joined: 2/3/2011 Last visit: 2/6/2025 Posts: 348 Rating:
|
Hi, I want to connect 2 s7-400(414) thorugh MPI to send some data. How can I do it? |
8/8/2012 10:37 PM | |
Joined: 9/27/2006 Last visit: 3/22/2025 Posts: 12344 Rating:
|
Hello syd; In the following FAQ you have a quick description of various types of exchanges over MPI and the system functions you use to generate them; you will also find links to sample programs for each: Options for communications via MPI The following link brings to to a very complete compendium of communication options between Simatic S7 CPUs. A good read if you want to go further than just recipes. Which protocols and services can you use for communication via MPI? Hope this helps, Daniel chartier |
Follow us on