11/13/2015 4:03 PM | |
Posts: 1 Rating:
|
Hi there, I´m trying to connect a PAC-4200 (Using a Switched Profinet 7KM9300-0AE01-0A00 V2.1) to read the values trought the Profinet. I´m using TIA Portal V13 and a CPU s7-1500 1) I already install the gsd file on TIA Portal 2) I found the module on Acessible Devices, Assign IP and ping to confirm. 3) When I go to add new devices (I believe that I need this to apply where I wanna read the values ex. %Ixxx on PLC) I cannot find this module or any kind of it. I just have PLCs, HMIs, PCs and Drive as option.
Thanks in advance Anderson ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/16/2015 11:55:18 AMNew subject after splitting |
|
11/15/2015 7:20 PM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello Anderson, pls do you use V13 SP1 with next updates? |
With best regards... |
|
Follow us on