6/9/2015 8:19 AM | |
Posts: 47 Rating: (1) |
dear all how can i connect or disconnect cpu 314 and cp341 and 2 DI and 2 DO on rack can anyone show me how can i do that thank you |
6/9/2015 9:20 AM | |
Posts: 47 Rating: (1) |
Sorry i mean on rail and what must change in program when i change from cpu314 to cpu315 only hw config |
6/9/2015 10:50 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, see following manual chapter 5 SIMATIC S7-300 CPU 31xC and CPU 31x: Installation This will be very helpfull for you, there are pictures where you see how they connected to the rail and each other. To change it in your project go to the HW-config and try with rigth-click on CPU, then click replace Object. you can also try to delete the CPU and try to Insert a new Object. But don´t delete your programm by deleting the old CPU. Don´t forget to make a Back-Up before start changing hope this helps, regards, |
FCK WAR! |
|
6/9/2015 12:19 PM | |
Posts: 47 Rating: (1) |
Thank you very much |
Follow us on