10/20/2015 9:08 PM | |
Joined: 11/29/2011 Last visit: 10/25/2023 Posts: 1348 Rating:
|
Hi, Start with this example: SINAMICS G: Connecting of a G120 (Startdrive) using S7-300/400 (TIA-Portal) with PROFIBUS and HMI Some more examples for TIA+S7-300/400+G120: SIMATIC Converting Toolbox winder and line tension control SINAMICS G/S: Configuration of standard telegrams in TIA Portal
|
- What you read here, please check with manuals and your requirements. |
|
10/21/2015 6:27 PM | |
Joined: 5/12/2006 Last visit: 12/5/2023 Posts: 21954 Rating:
|
then check the programming blocks which you can download here: https://support.industry.siemens.com/cs/ww/en/view/109475044 but note! with a programming block you can't connect a drive only control it at the moment it is not really clear if you have problems with the programming ot with the configuring. Regards Christoph |
This contribution was helpful to
1 thankful Users |
10/22/2015 4:17 PM | |
Joined: 5/12/2006 Last visit: 12/5/2023 Posts: 21954 Rating:
|
Hello, question 1: yes, you call this one FB in you OB and control the drive question 2: no Regards Christoph |
10/22/2015 5:36 PM | |
Joined: 5/12/2006 Last visit: 12/5/2023 Posts: 21954 Rating:
|
Hello, q1: if you use EPOS in SINAMCIS Telegramm 111, if not then 1 q2: Telegrams are the defined Datasequence for Communication between PLC and drive q3: SINA_POS = positioning Control of a drive, SINA_PARA = read/write drive parameters q4: no you must nout use this functions q5: systemfunctions to read and write data to a Slave Why you don't read the manuals? All questions are answered in the manuals and descriptions! Regards Christoph |
Follow us on