9/14/2022 8:14 AM | |
Joined: 3/18/2021 Last visit: 6/19/2023 Posts: 31 Rating:
|
Hi, thanks for your answer! Yes, the connection looks like in your graph. When I type "nmcli" it shows that both ports are connected. I can ping my PC 192.168.200.202 but not to the IO-Link Master 192.168.200.201. Attached are some outputs from IOT2050. Strange is, that I can't establish an SSH connection after rebooting when both devices are connected to the ports. Only after disconnecting the ethernet cable from P2, I can connect with my PC to the IOT2050. Even stranger is, that when I then plug in the IO-Master again, it connects for one moment with the Broker and I even see a message on MQTT Explorer. But after that, no more messages are sent. I hope this helps to find the problem. I don't know where the reason could be. Thanks in advance and best regards! Attachmentproblem connection.zip (145 Downloads) |
9/14/2022 9:32 AM | |
Joined: 6/8/2018 Last visit: 11/30/2023 Posts: 94 Rating:
|
Hi ! Master IO link -> Pub in 192.168.201.1 P2 IOT Attachmentshema.zip (194 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on