6/30/2016 3:35 PM | |
Posts: 2 Rating: (0) |
Thank you for your answers, I have the manual from the TeSys and they are variables predefined who I can used in the program, but what I want it´s call a register from the TeSys to the PLC, that register will be 457 or 700 or whatever I want. That´s the part of programming of PLC. The document that I attached it´s from the TeSys T and they are the images from the format big endian and how to call the registers but I tried without success, the words IW0 to IW8 work good but when i work with the PKW I mean with the words IW10 to IW16 doesn´t do anything, if you could help me to understand it and how put it in the PLC I will aprecciate it, thank you for all your answers and have a nice day.
Attachmentprofibus tesys variables.pdf (372 Downloads) |
Follow us on