6/25/2016 10:55 AM | |
Posts: 45 Rating:
|
Hello Daniel, I need your help to connect three s71200 plc in which master PLC S71215C with CM1243-5 and remaining two S1214c with CM1242-5. I want to know the steps of communication, data tranfer block and how can we transfer status from two 1214c filed plc to master and control status from master 1215c plc to filed. Thanks!
------------------------------------------------------------------------------------------ AttachmentStructure.pdf (309 Downloads) |
Last edited by: Min_Moderator at: 6/27/2016 3:20:39 PMNew subject after splitting |
|
6/25/2016 12:13 PM | |||
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello vaggmin, Is the same queston?
|
||
Last edited by: Ste39 at: 6/25/2016 12:13:57 PMLast edited by: Ste39 at: 6/25/2016 5:19:53 PMMy mistake PUT/GET :-( Last edited by: Min_Moderator at: 6/27/2016 3:23:03 PMChange link |
|||
7/3/2016 2:51 PM | |
Posts: 45 Rating:
|
Is it possible to connect two S71200 PLC on ethernet in between distance 125Mtr. If not then how can i do that.
|
7/3/2016 9:02 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, Industrial Ethernet the maximum distance is ca. 100 meters you can use a switch or optical |
Follow us on