11/14/2016 7:00 AM | |
Joined: 1/2/2014 Last visit: 4/16/2025 Posts: 150 Rating:
|
Please check the LINK HERE. MPI will support 31 nodes but length is limited to 50 meter. PC's must have a CP card [like CP 5612]. |
This contribution was helpful to
1 thankful Users |
11/15/2016 11:26 AM | |
Joined: 7/9/2015 Last visit: 4/17/2025 Posts: 4249 Rating:
|
Hi, I know these FAQ - hope this helps you: How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?Regards, Towome |
|
|
This contribution was helpful to
1 thankful Users |
11/15/2016 11:38 AM | |
Joined: 11/14/2016 Last visit: 8/27/2024 Posts: 5 Rating:
|
but i have Wincc 7.1 not Wincc flexible.
|
11/15/2016 11:42 AM | |
Joined: 11/14/2016 Last visit: 8/27/2024 Posts: 5 Rating:
|
Can you explain the wiring of that, how i can take two link (wire) of one port on CP 5612?
|
11/15/2016 2:37 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello sajjad; MPI is a subset of Profibus networks, and uses the same RS-485 cabling infrastructure, daisy-chaining the elements of a network. RS-485 cable (shilded twisted-pair) and sub-D 9-pin connectors are easy and cheap to locate (connect pins 3-5-8 on each connector), and termination resistance can be implemented with a bit of thought. But generally we prefer using Profibus connectors and cables, a bit more expensive but all elements are certified (so they will work as expected without a problem) and termination circuits are already built-in. See the attachment for an illustration, and this list of Profibus connectors part numbers (from Siemens; there are many manufacturers offering similar connectors, such as HelmHoltz, ABB, Phoenix Contacts...). Where can you find information on the dimensions of PROFIBUS connectors and where can you find dimensioned drawings of the PROFIBUS connectors? https://support.industry.siemens.com/cs/fr/en/view/19425126 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/15/2016 4:06:30 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on