2/22/2011 1:04 PM | |
Posts: 40 Rating:
|
Dear sure Thank you very much for your advice I want to ask about something I found After searching the Wincc flixible2008 I found that I can make 8 connections to 8 separated s7-200 CPU’s and using PC Access as an OPC I can also made a connection t 8 CPU’s So I tried using Wincc and PC Access to make a connection to the OPC ( that has 8 connections) from wincc and three other connections from Wincc to the last 3 other S7-200 CPU’s And WinCC accepted that ( note the attached image) And is this can be done from the same Station (connecting Wincc to an OPC on the same PC and 3 other CPU’s)? I need your advice about using this method Note: My network is MPI using CP5611 Thank you very much Splitted from Connecting Wincc with PC Access and 3 other S7-200 CPU's. |
Last edited by: O_Moderator at: 2/22/2011 1:22 PMnew subject after splitting |
|
2/22/2011 1:23 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread Connecting Wincc with PC Access and 3 other S7-200 CPU's. Best regards O_Moderator |
Follow us on