12/3/2015 10:10 AM | |
Joined: 7/9/2015 Last visit: 3/14/2025 Posts: 4198 Rating:
|
Hi,
if your PLCs have an integrated Profinet interface you could use the open user communication using TCON, TSEND... This TCP connection must not be configured in NetPro and you must not change the HW configuration. Look here: How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU? https://support.industry.siemens.com/cs/de/en/view/29737950
Hope this helps, Regards, Towome |
Last edited by: Towome at: 12/3/2015 10:11:43 AM
|
|
12/3/2015 11:44 AM | |
Posts: 15 Rating:
|
I look at this manual, but there are changes on netpro. Because of that i need to download new hardware configuration and i dont want to do it.
|
12/4/2015 8:35 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi primoz, I don´t know were you are lookin at!? The FAQ and the procedure, Towome shared with you, is a programmable communication, compared to a configurated communication like S7-communication. You don´t have to change something in HW-config or Netpro. There is only a need to load some blocks and implement it in your programm. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
2 thankful Users |
Follow us on