11/13/2019 9:46 PM | |
Posts: 2 Rating: (1) |
Hi, there seems to be a mistake in Siemens documentation with regard to multi phase connection for the LOGO! 230RCE inputs. I checked multiple documents and they contradict each other or even themselves regarding this question. I understand that you can't mix the phases within the same group of four inputs. But it is not clear what phase can you use for power supply (L1) of the base and expansion modules. According to the diagram on page 48 of the Logo Manual (https://support.industry.siemens.com/cs/attachments/109741041/logo_system_manual_en-US_en-US.pdf?download=true) power supply (L1) can be different phases for the base module and expansion module. But according to the caution on the page 41 the phases for L1 of the base and expansion module must be the same! According to this document (https://assets.new.siemens.com/siemens/assets/public.1542881817.f583a4ec-cfaa-4e6f-a931-0cbcb5d3652a.go182-en-gewusstwie.pdf ) the power supply (L1) can be different for the base and expansion module BUT the power supply must come from the first group of inputs on the module! But according to page 8 of this document (https://support.industry.siemens.com/cs/attachments/109755865/109755865_LOGO8_TDE-CentralControl-RollerBlinds_en.pdf) the power supply (L1) must be the same for all modules and doesn't have to come from the first group of inputs. All the documents can't be right because they directly contradict. Logos are part of my house automation project. I am using LOGO! 230RCE basic module with two DM16 230R expansion modules. All the inputs on the basic module and the first expansion module will be connected to phase L1. But the groups on the second expansion module will be connected to different phases (group 1 to L2 and group 2 to L3). What phase do I connect to the power supply of the second expansion module? |
Follow us on