Industry Online Support
Technical Forum
4/18/2009 12:23 AM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308) |
Hello Hozgur, I don't have experience with this module but if you take a look at S7-300 module data at page 243, you will find that this module can't measure resistance directly. It can measure only Voltage & Current. However, you can use the POT as a voltage divider. In this case you will have to use an external voltage source (5V or 10 V for example) and connect it through your POT to the same pins as if you were using module to measure voltage. You can see a similar connection for6ES7 331-1KF01-0AB0 in page 271(channel 7). The pins in your module will be 38 and 40 (Channel 7). I think it will work. H-H |
Follow us on