Industry Online Support
Technical Forum
12/17/2009 8:32 AM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, I`m a little confused. What do you want to do???? Which components you use??? S7-300, S7-400, S7-200??? Which bus system do you have ?? PROFIBUS, Ethernet, Wireless???? You have written about GSM and Wireless... Do you haveheard of SINAUT, yet???Maybe it`s a solution for you... "SINAUT® ST7 is a system based on SIMATIC® S7 for fully automatic monitoring and control of process stations that exchange data with another and with one or more control centers over a WAN (wide area network) or Ethernet (TCP/IP)." In the manual you find more information about area of application, possible network topologies and the components in a SINAUT ST7 system. http://support.automation.siemens.com/WW/view/en/39026870 |
Follow us on