8/27/2008 6:15 AM | |
Posts: 487 Rating: (36) |
amk This seems like a big contract .I would suggest you to contact Siemens en let them spell out the options.Download this manual ,its all about converting from S5 to S7( see page 2.9) If you want to keep the exisiting IQ make sure the extension racks only contain digital input and outputs.Analog may give you problems and any other card ( ie counters,comms) are not supported. Also if you are going to use PCS7 then you cannot convert the software , its a complete rewrite and there are no shortcuts you can take.I hope the documentation is 100% Eric |
Follow us on