Industry Online Support
Technical Forum
1/31/2013 12:54 PM | |
Posts: 24 Rating:
|
Hello, Is it possible to Connect TP177B and OP25 to 928B (im308)(S5 DP) ? I have done everything like here: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=31676209&caller=view But TP177B shows connectionerror, and OP25 loose some data. When I turn off communication with OP25 in PLC (not in ComProfibus) - there were no errors on TP177B, but values were showed for some short period, and then: "#####" I alsoconnect TP177B with 944 (just two devices on profibus for test purpose)- it works well. Thanks for any answer. |
2/4/2013 2:07 PM | |
Posts: 3037 Rating:
|
Hello, See the followings links: Connecting a Windows-based panel to an IM308C (SIMATIC S5) via PROFIBUS DP How is the connection between a Windows-based panel and a SIMATIC S5 set up? Tweety |
2/7/2013 8:10 AM | |
Posts: 24 Rating:
|
I have done it like these links says. Next week I will try with totaly disconected OP25. thanks for reply |
Follow us on