5/27/2021 8:49 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
you don´t need a factory reset for that., occupied connections will be reset just by power off/on. The actual FW also has a function called Keep-Alive-connection monitoring, keepalives are sent for connections via TCP/IP. This ensures that connections are terminated if one of the communication partners fails and that connection resources are released again. furthermore I think this has another reason. When you are able to connect over online devices, you are also able to connect with project. I would rather check if you are in the rigth IP-range with your Programming device. Also try it over extended online connection and directly to the IP, the CPU has, as shown in this FAQ: How can you use the STEP 7 Online functions even when NAT (Network Address Translation) is being used or a remote subnetwork is to be reached?hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |