7/2/2015 11:10 AM | |
Joined: 11/30/2012 Last visit: 9/10/2024 Posts: 1 Rating:
|
At first I need to do a CPU to CPU data-exchange by using GPRS from Scalance M874-3, like the below picture.(My config) In my config don't have any PC in network. I already 2 x SIM fix IP address of Scalance M874-3. Could someone tell me can I config the network like the picture(My Config)? P.S. I haven't mind if it not VPN Tunnel. You can tell any method. Thank you, |
This contribution was helpful to
1 thankful Users |
10/8/2015 8:45 AM | |
Posts: 1 Rating:
|
Hi,BeCkKiE Are you done with this solution.Can you tell me how to do? |
6/16/2016 3:32 PM | |
Posts: 6 Rating:
|
Hey BeCkKiE, Do you have any result so far? Would be great to send a a feedback. |
8/28/2017 7:57 AM | |
Joined: 8/21/2014 Last visit: 3/18/2025 Posts: 1036 Rating:
|
New question published by esteban.idro is split to a separate thread with the subject Connection between 2 Scalance M874-3 module. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on