11/14/2014 5:24 PM | |
Posts: 5225 Rating: (1185) |
Hi there, A recent discussion needed the pin layout of a cable between S7-200 and TD200. Maybe this is of value to you [LINK]. IN my opinion you should look for the answer at the 3rd party panel's web site or support forum. Especially the Turkish Language forum might be of help. Sometimes that answer is already part of the program that you use for creating the program for the panel.. look for "PPI" or "S7-200". What I will say is that some panels have very funny connection with S7-200 PLC so make double sure of the facts - especially when it comes to the cable shield. What you should remember also is that you need to specify in the panel program to which PLC the panel is talking to. Agin it might be "PPI" or "S7-200". This is what I can offer until someone who actually worked with this combination come forward. Greetings. w |
Follow us on