6/26/2015 3:38 AM | |
Joined: 9/29/2014 Last visit: 3/18/2025 Posts: 1 Rating:
|
Hi everyone, I'm working on a project, to connect 1 s7-300 plc with 2 s7-1200 plc i use this program provided by siemens: https://support.industry.siemens.com/cs/document/40556214?dti=0&lc=en-WW All PLC are connected via a switch I did add some block and change the DB and FB numbers to match with my project, i tested it and it worked fine. After that when my friend add his program into the s7-300 it still worked fine. However when we test it again yesterday, it stopped working. I tried to load the original test program that i included here and it still not working. The s7-300 "Get" instance just output Error and status W#16#0001. The manual said faulty wiring was caused this problem, however i think the connecting wires is OK since I could online all the plc with TIA portal. I'm confused here, i think maybe my program is wrong? Anyone can help me solve this problem? AttachmentS7-Comm_Sync_V13_Test_OK_9-6-2015.rar (72 Downloads) |
Last edited by: ductue at: 6/26/2015 3:41:27 AM |
|
Follow us on