6/19/2009 9:13 AM | |
Joined: 1/26/2007 Last visit: 3/8/2025 Posts: 123 Rating:
|
I have found an list with many panels and also the connections for them . from the table seems to be ok the cable that i have made for OP7 . Now i do not know what to belive . is ok the serial cable (that i have built and used Ok for an OP7 ) to use Ok also to an OP 37 ?? AttachmentProjekttransfer_e_C1.pdf (807 Downloads) |
6/19/2009 9:16 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hi, Look at What transfer options are available in the various operator panels? Regards Hristo Mihalev |
Last edited by: UMENCHO at: 6/19/2009 9:23 AMWhat is exactly your type, I mean MLFB number. |
|
6/19/2009 10:49 AM | |
Joined: 11/21/2007 Last visit: 3/16/2025 Posts: 2326 Rating:
|
Hi You can assemble the RS232 Serial Cable for Download to OP37 yourself. We have been using these without any problems for a long time for most of old TD/OPs including OP37 Best Regards Navnag AttachmentPG_OP_RS232_Cable.PDF (1018 Downloads) |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
3 thankful Users |
Follow us on