3/22/2017 8:45 AM | |
Joined: 4/28/2015 Last visit: 2/25/2025 Posts: 70 Rating:
|
Hello everyone! I realy need your advices! I must communicate with RISC PLCs of clients according rs232 interface. They wants to use special device NPort5200 - it is converter rs232 - to ethernet NPort5210A.PDF . My CPU is 313C with modul CP 341-RS232C For first i made all settings of cp341 like in this manual SETUP CP341 .Pdf page 14. Then i connected both device with special cable rj45-db9 (female), wires diagram are in my attachments. I am using functions P_SND_RK to send data and P_RCV_RK for recieving . But i have no result. Leds on the module cp341 always off, when i swith 0->1 request bit (P_SND_RK) nothing still no effect. But when i disconect the cable led SF became RED. If i send some data into CP341 i must see TX blinking, is't it? I attached image of the online status of the my module and pogram. Pls, can you pay attention for my question. MAy be i made something wrong. With best regards, Dmitry. Attachment1.pdf (179 Downloads) |
3/22/2017 2:06 PM | |
Joined: 4/28/2015 Last visit: 2/25/2025 Posts: 70 Rating:
|
|
Follow us on