1/14/2016 9:40 AM | |
Posts: 4 Rating: (1) |
Hello everybody, I have new CPU 313C with HMI ( LS - XP30BTE ). In start of the project , I connected to the CPU and downloaded the project in CPU , then Connected to the HMI and downloaded the HMI project , finally connecting HMI to PLC but seen message " Connection time out " Now when connecting to CPU as PC again , see the message : " 33:16944 Online: No other active Partner can be found " My PC Adapter is : PC Adapter USB A2 I can connect to any CPU by current PC Adapter . Please help me . HMI Communication DOC : http://lsis.biz/common/handler/download.ashx?path=/upload/customer/download/1423/XP%20Communication_Eng_V2.2.pdf.32812 Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/14/2016 1:34:06 PMNew subject after splitting |
|
3/11/2016 11:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by problem plc is split to a separate thread with the subject Format MMC, Error "No other active partner can be found". Best regards |
This contribution was helpful to1 thankful Users |
Follow us on