5/18/2020 6:34 PM | |
Joined: 2/5/2013 Last visit: 5/21/2024 Posts: 320 Rating: (74) |
Hi ppwhk, It will be more helpful if you attach screenshot for below information. 1.Installed Software Portal View-->Installed Software--->>Detailed Infromation about Installed Software 2.Which Windows 10 Version and OS Build 3.Check from which TIA version Old PLC Code downloaded in controller Project View --->> Online Access --->> Select Proper Driver --->> Update Accessible Devices -->> Select Controller -->> Online & diagnostics -->> Diagnostics -->> TIA Portal Project Version. 4.Check IP address assigned to PG/PC with different IP address than PLC addess and should be in same subnet 5.Error Message. Br, AmolG. |
Please rate it. |
|
5/18/2020 7:36 PM | |
Joined: 3/30/2020 Last visit: 5/22/2024 Posts: 4524 Rating: (944) |
Hello. Windows 10 can do some strange things to HELP the user. Additionally - Set the IP address to a fixed address. Test if it make any difference. BR |
Last edited by: qwazee at: 05/18/2020 19:37:33Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
5/19/2020 10:28 AM | |
Joined: 11/26/2018 Last visit: 6/7/2022 Posts: 11 Rating: (0) |
The problem is the ip-adress. In the attachment : how can I change the IP adress. Change settings is unlighted. |
5/19/2020 10:32 AM | |
Joined: 11/26/2018 Last visit: 6/7/2022 Posts: 11 Rating: (0) |
Edimax Edimax EU-4208 At school, it works on windows 10 |
5/19/2020 10:47 AM | |
Joined: 2/5/2013 Last visit: 5/21/2024 Posts: 320 Rating: (74) |
Please find attached Pdf. Select Particular driver from control panel > Network and Internet > Network Connections I think in your case it is Edimax usb converter Br, AmolG AttachmentIP.pdf (90 Downloads) |
Please rate it. |
|
This contribution was helpful to1 thankful Users |
5/19/2020 9:54 PM | |
Joined: 11/26/2018 Last visit: 6/7/2022 Posts: 11 Rating: (0) |
I set the ip-adress correct (see attachment) but connection still fails. What is wrong? AttachmentThe IP.pdf (75 Downloads) |
5/19/2020 10:12 PM | |
Joined: 2/5/2013 Last visit: 5/21/2024 Posts: 320 Rating: (74) |
Hi ppwhk, I hope you are selecting proper version for Unspecified device.Please find attached Image for Version selection. Have you downloaded program in controller previously then we need same version of TIA. Br, AmolG |
Last edited by: AmolG at: 05/19/2020 22:13:20Please rate it. |
|
This contribution was helpful to1 thankful Users |
5/20/2020 2:47 PM | |
Joined: 11/26/2018 Last visit: 6/7/2022 Posts: 11 Rating: (0) |
I want to detect the type of plc but the problem is it the connection doesn't work when I press detect. |
Follow us on