Industry Online Support
Technical Forum
9/21/2011 10:49 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, at this link you can find the communication manual for flexible. There at chapter 4.1 the communcation via LG PLCs. SIMATIC HMI WinCC flexible 2008 Communication Part 2 In this case you can just ask at LG if the released PLCs for the communication with the panel uses the same base, or are they similar. best regards. |
Follow us on