8/6/2015 10:41 AM | |
Joined: 10/18/2013 Last visit: 12/27/2024 Posts: 3 Rating:
|
2015. PG M4 with Win7 64 bit + Step 7 5.5 SP4 and the same problem. Please help:)!!! |
8/6/2015 11:00 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, Have you tried to turn it off and on again? ...just a joke have a look in the services your Win7 is running. You will find them in system-control. There is a service that should work, normally automatically, called SIMATIC S7DOS help Service. if this solution doesn´t fit, you can try to initialize your interface drivers. See following FAQ: How do you assign the parameters of the PG/PC interface in general and what is the remedy if the device driver cannot be selected or is not visible?hope this helps, regards, |
FCK WAR! |
|
Follow us on