1/26/2015 4:14 PM | |
Joined: 4/24/2006 Last visit: 2/17/2025 Posts: 8850 Rating:
|
Hello, Have you seen this link: how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Can you give the MLFB number of used OP73? Best regards, Wizard |
1/26/2015 4:24 PM | |
Posts: 1058 Rating:
|
Some Links that might be helpful: How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? OP73 profibus setting MPI Connection between CPU313C and 3 OP73 Operating Panels OP73 pb reconnection and detection regards |
1/27/2015 9:21 AM | |
Posts: 7 Rating:
|
In your last link, the user has exactly same problem as mine !!! Regards, Jpp. |
1/27/2015 10:15 AM | |
Joined: 4/24/2006 Last visit: 2/17/2025 Posts: 8850 Rating:
|
Hello, when you have a look at the following link: how do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? Have a look at page 8 of PDF. See note. Highest node address should be 63 or less. (Bear in mind, this should be on the whole profibus network) Best regards, Wizard |
Follow us on