12/28/2010 6:02 PM | |
Posts: 14 Rating: (0) |
basp led is red run led is off stop led is flashing what is the problem and how to make aconnection between pc and (S5 CPU928B) best regards |
12/28/2010 6:50 PM | |
Posts: 510 Rating: (117)
|
This should be in the S5 Product conference billwest |
12/28/2010 7:43 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, You should do a overall reset (Performing an OVERALL RESET) and then to download the program. About connection between PC and CPU you need Step5 software, PG and cable. Look at S5-135U CPU 928B Programming Guide Best regards, Hristo Mihalev |
12/29/2010 12:55 AM | |
Joined: 10/7/2005 Last visit: 10/13/2024 Posts: 3024 Rating: (1054)
|
Hello draz before you decide to do the overall reset, please check first at what frequency the Stop LED is flashing. If its flashing fast (~ 2Hz), then the CPU does indeed request an overall reset. If its flashing slow (~ 0.5Hz), then the CPU does NOT need anoverall reset, but can instead be restarted with a so called "Cold restart" (it may of course go back into Stop again if the orginal cause of the CPU Stopstill exist). Whiel I can't tell you what caused your CPU Stop, I can tell you that a good place find this out is the Istack and chapter 5 of the CPU manual that UMENCHOpointed you too has all the details on how to evaulte the Istack (see alsochapter 4 for all things stop,restart and run mode related). Let us know what you find and come back here with more questions. I hope this helps |
Cheers |
|
1/2/2011 9:26 AM | |||
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181)
|
Hello, Perhaps this might helps you
Best regards, Hristo Mihalev |
||
1/3/2011 5:38 AM | |
Posts: 14 Rating: (0) |
thanks so much for helping us |
Follow us on