6/3/2016 8:28 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Craincross, your problem relates not only to this one CPU(315-2AG10), rigth? If it does, the problem is on the CPU-side und I would try to reset the CPU to factory settings. In following manual you can read how to do it: SIMATIC S7-300 CPU 31xC and CPU 31x: Installation chapter 9.5 If you can´t connect to any CPU, wo have to search on programming-device. Try to reset the PG-interfaces, This FAQ will help: hope this helps, regards, |
FCK WAR! |
|
6/3/2016 9:04 AM | |
Posts: 18 Rating:
|
correct it relates to 7 plc's in total, in the past to check online connection all that was required was make a new project set CP5611 to auto and up load, also going online to do comparison with stored program on PG/PC this has only occured since trying to log onto the CPU315 2DP, I think there is something qrong with it and it has cause a problem in the hardware I will read through the SIMATIC installation manual shortly thanks for the feed back |
6/4/2016 3:28 AM | |
Posts: 18 Rating:
|
Here are a few test i tried with different settings |
6/4/2016 3:29 AM | |
Posts: 18 Rating:
|
this is with DP selected |
Follow us on