12/3/2014 5:43 PM | |
Posts: 5225 Rating:
|
Hi there.
Please have a look at [LINK] for a full description of the above. Also look at the functions that has been added to firmware 4. If you do not need to have firmware 4, I suggest for you to come in contact with the company that sold you the unit. See if you and them can maybe come to some sort of agreement for getting hold of the firmware 3 version of PLC. These are available in parallel (V3 and V4). Another option is to get an upgrade licence to go to TIA13. Even using a demo version of TIA13 is possible for you (20 or so days). Anything else is to welcome insanity to your doorstep. w |
Follow us on