9/27/2016 10:50 AM | |
Posts: 7 Rating:
|
Amy, thanks for detailed explanation. I am concerned about connection to s7-1200 and s7-1500! Do these models have direct Ethernet module for LAN connection and no additional interface/hardware is needed. Regards, Goce ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/27/2016 11:58:42 AMNew subject after splitting |
|
9/27/2016 12:52 PM | |
Joined: 7/9/2015 Last visit: 2/3/2023 Posts: 3289 Rating:
|
Hi, this FAQ could also be interesting for you: With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols does the S7-1200 support?Regards, Towome |
If my post was useful, please rate me - thank you! |
|
Follow us on