8/27/2020 7:39 PM | |
Joined: 1/3/2018 Last visit: 10/23/2024 Posts: 33 Rating:
|
Hi all, I'm using TIA Portal V15.1 Upd4 for WinCC Advanced Runtime for programming Comfort Panels. I have always used "absolute access" as a configuration for my tags, for backward compatibility reasons and for the convenience of using structured faceplates (ie with HMI UDT in the interface). Now I'm working on a project that doesn't require their use and, if necessary, I can define dedicated tag tables for that feature. So I'm wondering what constraints are involved when we use this type of access mode (handling, linking, use in scripts, ecc.). --- Edit --- Watching through the forum I found this hint but I'm not sure that is right. Can I have a confirm on this : https://support.industry.siemens.com/tf/it/it/posts/hmi-udt-vs-plc-udt/128832/?page=0&pageSize=10
Because I tried to follow this method but without success. --- Edit --- Thanks for the help and best regards. |
Last edited by: Corn98 at: 08/28/2020 11:15:49 |
|
9/9/2020 3:51 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello yes since V13 SP1 your can use PLC UDTs direct in Facelate interfaces (But only with S71200/S71500). A quite good explaination is in this FAQ: https://support.industry.siemens.com/cs/ww/en/view/68014632 If you cannot get it work then please send us a few screenshot what steps you have trouble with. Bye Murof |
Last edited by: Murof at: 09/09/2020 15:52:10If this Information really helps, you could use the Rate function |
|
Follow us on