10/31/2012 7:35 PM | |
Joined: 3/2/2009 Last visit: 8/6/2024 Posts: 94 Rating: (8)
|
Dear vipz, you have to transfer the license back to eg. USB-Stick. I would recommend to use attached Restore-DVD for installation - you would not need to install additional driver because in the image everything needed is enclosed. Driver installation is necessary if you use Recovery-DVD. You will find information about installation in the operating manual: http://support.automation.siemens.com/WW/view/en/34072142 12.8.2.2 Restoring the Software to Factory State Using the Restore DVD .... 149 12.8.2.3 Setting up the operating system via the Recovery DVD.... 150 |
11/2/2012 5:41 AM | |
Joined: 3/2/2009 Last visit: 8/6/2024 Posts: 94 Rating: (8)
|
Dear vipz, what information do you need concerning "contract license"? Did you have a look at attached CDs/DVDs? Regs, grg |
Follow us on