8/26/2014 5:02 PM | |
Joined: 11/7/2013 Last visit: 10/7/2024 Posts: 32 Rating:
|
Email form Balluff Tech Supp: "Changing the SPDU to get another function like "Level Mode" or "Runlight Mode" you need the IO-Link Function Block from Siemens. I´m wondering why they don´t know it. In attachment you will find a sample project and manual for TIA12, I´m not sure if all functions will be supported at TIA11. If not the problem can be the basic version of TIA11, with TIA 12 or 13 are more functions available." Therefore im asking, is it possible to configure my device using TIA11 update 3, where i dont have IO_Link_Call function block? AttachmentBNI_PNT_IOL_Siemens_FB1_TIAv12_1200PLC_2013-11-25_E.PDF (1068 Downloads) |
Follow us on