11/23/2010 6:38 AM | |
Joined: 10/11/2010 Last visit: 2/27/2024 Posts: 6 Rating: (0) |
Hello everybody! I have some problem to control third party motor. I want to control ETEL Torque motor(DD motor) with 840D SL. The ETEL motor rated speed is 280 RPM but I want to let this motor reach 800 RPM. The ETEL engineer tell me that this motor need control with field-weakening to reach 800 RPM. I know field-weakening theorem but I don't know how to set parameter for 840D sl. If any one ever meet this problem like me, can you tell me how to do. Thank You! PS: The attachment file is ETEL DD motor datasheet AttachmentETEL TMK0360-150-3UFN-data-v1.1.pdf (148 Downloads) |
11/23/2010 10:06 AM | |
Joined: 1/19/2008 Last visit: 10/2/2024 Posts: 992 Rating: (64) |
Hi, Are you connecting this motor to a Siemens drive module or has it got it's own drive unit ?. Pee |
1/5/2011 2:30 AM | |
Posts: 8 Rating: (0) |
Up! I also want to know. |
1/25/2011 1:23 AM | |
Joined: 10/11/2010 Last visit: 2/27/2024 Posts: 6 Rating: (0) |
This problem has been solved. Thank you every body. |
Follow us on