7/11/2010 11:04 PM | |
Posts: 14 Rating:
|
how can i download and upload from plc s7_1214 through the internet if this .......osible please help me ? |
7/12/2010 9:07 AM | |
Joined: 3/21/2006 Last visit: 3/14/2025 Posts: 10239 Rating:
|
Hello, Yes, its possible to have connection to the S7-1200 via Internet. You need to assign router IP address of CPU. Then in router you should set this IP address and build VPN connection which will connect both sides. About VPN connection look at How is a VPN tunnel between two SCALANCE S S 61x modules configured in Routing mode via the Internet? Best regards, Hristo Mihalev |
Follow us on