6/9/2021 1:19 PM | |
Joined: 7/25/2017 Last visit: 4/5/2025 Posts: 7 Rating:
|
Dear Experts , Kindly provide clarity and support on these points according which we have observed in WINCC with OPC Channel 1. After filling control parameters and switching to another screen value has been zero. 2. After filling control parameters and Deactivate runtime then value has been zero. 3. After filling control parameters, shut down the PC and Restart then value has been zero. 4. After filling control parameters, remote station Disconnected and reconnect then value has been zero. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/09/2021 14:01:06New subject after splitting |
|
6/10/2021 11:35 AM | |
Joined: 10/10/2014 Last visit: 11/13/2024 Posts: 1725 Rating:
|
Hi Titu1, If i understand correct the communication problem happen only with WinCC V7.4 SP1 and not with WinCc Advanced, WinCC Professional and OPC Scout. Witch WinCC V7.4 SP1 update do you use on your system ? May be it helps to install the latest WinCC V7.4 SP1 update See Update 17 for WinCC V7.4 SP1 and WinCC V7.4 SP1 ASIA https://support.industry.siemens.com/cs/de/en/view/109794344 If the update not help collect the diagnostic files with the SAS tooll and open a service request for SIEMENS Support Best regards schufri |
Follow us on